Saving a Graphic

When you have created a graphic you can save it to the database.

To save a graphic:

  1. In Graphics Editor, on the File menu, click Save.

NOTE: You can only save a graphic in Preview mode. If you choose to save by using the Save As command, the link to the database is broken and you have to define the location where you want to save the TGML graphics file in the file system.